Configure the AKD / AKD2G Drive

The Configuration tab under the EtherCAT: AKD tab is used to configure drives once these conditions have been met:

You then have access to all of the AKD configurations and parameters.

  1. In the Project Explorer, double-click the new AKD Drive or select Configuration from the context menu to open all the parameters linked to it.
    AKD Configuration
  2. Figure 1: AKD Configuration

  3. Define the motion parameters in the Limits tab to configure the limited motor torque, speed, and acceleration

  4. Define the motion parameters in the Position Loop tab to configure the limiting error.

  5. Define the resolution of the feedback position in the Feedback tab.
    For all feedback types, the motor position feedback sent from the AKD drive to the controller through EtherCAT is normalized to 20 bits/rev or 1048576 counts/rev.
  6. Define the units used for the motion 1:

    • User units in the PLC language editors are:

      • Position: User unit
      • Velocity User unit/sec
      • Acceleration: User unit/sec2

      Several AKD tabs contain units that follow the standard AKD format:

      • Position: 16 bits/rev
      • Velocity: RPM
      • Acceleration: RPM/ Sec
  7. To ensure high performance, define the load for your servo system.
    KAS-IDE provides several options for performing the drive tuning:
    • Slider Tuning - Use the slider to adjust to a designated bandwidth (pre-calculated tuning).
    • Performance Servo Tuner - Takes the drive through an automatic tuning sequence.
    • Manual Tuning - Used to set gains individually for:
      • Current Loop
      • Position Loop
      • Velocity Loop
  • See AKD Drive Configuration for more information about AKD configuration.
  • See the FAQs for more information about AKD Firmware Download.